CIMPLICITY REST API Web Service
CIMPLICITY REST API Web Service / CimSQLConnection Json Schema
CimSQLConnection Json Schema
Description
Fields that describe the connection to a SQL connection
Overview
CimSQLConnection
Fields that describe the connection to a SQL connection
ConnectionType : CimSQLConnectionType
ODBCDataSource : string
ODBC Data connection.
UserID : string
User who will connect to the selected database driver. A database user name is required if you are connecting to a SQL Server.
Passsword : string
Password needed to connect to the selected database driver. A password is required if you are connecting to a SQL Server.
ReconnectWaitPeriod : integer
The amount of time that the Database Logger waits between reconnect attempts when the connection to the database is lost.
ReconnectWaitUnit : CimTimeUnitEnum
defines units for time values
EnableStoreAndForward : boolean
Choose enable store and forward to enable the ALARM_LOG table perform store and forward options.
MaxNumberOfStoredRecord : number
To select the number of records the Database Logger will store when its connection to the database is down. Enter a number between 1 and 4294967285. 0 indicates no limit.
Properties
NameDescriptionData Type
 CimSQLConnectionType
ODBC Data connection.string
User who will connect to the selected database driver. A database user name is required if you are connecting to a SQL Server.string
Password needed to connect to the selected database driver. A password is required if you are connecting to a SQL Server.string
The amount of time that the Database Logger waits between reconnect attempts when the connection to the database is lost.integer
defines units for time valuesCimTimeUnitEnum
Choose enable store and forward to enable the ALARM_LOG table perform store and forward options.boolean
To select the number of records the Database Logger will store when its connection to the database is down. Enter a number between 1 and 4294967285. 0 indicates no limit.number
See Also